DALLAS, June 21, 2016 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) today introduced three high-performance retimers which enable an extended signal range over long traces, connectors and cables without degradation of signal integrity. These devices expand TI's high-performance retimer portfolio, and support flexible, cost-optimized system design, enabling designers to speed their products to market while maintaining optimal performance. With up to 60 percent lower power consumption than competitive devices and the widest temperature range from -40C to 85C, the new retimers enable robust video and camera signal quality in equipment such as desktop and laptop PCs, mobile devices, high-definition televisions (HDTVs), and automotive infotainment systems. For more information about TI's retimer portfolio, see www.ti.com/hdmi20-pr.
Key features and benefits of the new low-power retimers
- Leading jitter compensation: The new retimers improve signal quality by removing jitter and compensating loss for signals transmitting over long traces and cables. The DP159 and TMDS181 retimers include adaptive equalization (EQ) up to 15dB, dynamically adjusting the EQ level to fine tune system performance and enable better jitter compensation. The devices support multi-gigabit signals, such as DisplayPort and HDMI, up to 6 Gbps and operate at an extended temperature range, enabling designers to optimize performance in a wide variety of consumer, automotive and industrial equipment.
- Industry-leading system design flexibility: Various speed and protocol options, reprogrammable channel configuration, and scalable pin-to-pin compatibility for 1.4b and HDMI 2.0 devices enable engineers to design cost-optimized solutions with the lowest power consumption available today, up to 60 percent lower than competitive devices.
- Increased bandwidth: The DPHY440 device is the industry's first 4-by-1-Gbps MIPI camera serial interface (CSI) and display serial interface (DSI) retimer, providing over 10 times higher bandwidth than existing solutions enabling higher resolution camera images over long traces and cables.
- Optimize system performance: The DP159 and TMDS181 devices include robust features such as a pseudorandom binary sequence (PRBS) generator and real-time diagnostic EyeScan tools for in-system validation, which engineers can configure to quickly optimize their system design.
Package, availability and pricing
These new devices in TI's retimer portfolio are available with a variety of features, package types and pricing listed in the table below. Additionally, evaluation modules (EVMs) are available to help engineers quickly and easily evaluate performance and speed time to market.
Product |
Package options |
Pricing in 1,000-unit quantities |
EVM |
28WQFN |
Starting at $1.73USD |
||
28WQFN |
Starting at $1.50USD |
||
40WQFN 48VQFN |
Starting at $4.08USD |
||
40WQFN 48VQFN |
Starting at $3.55USD |
||
48VQFN |
Starting at $3.55USD |
Learn more about TI's retimer portfolio
- Check out TI's comprehensive portfolio of retimers.
- Read the Analog Wire blog post, "HDMI 2.0: How to generate cleaner signals over long traces, connectors and cables".
- Read the whitepaper, "Build a true fidelity system using video signal conditioners".
Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Photo - http://photos.prnewswire.com/prnh/20160620/381365
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/ti-introduces-the-industrys-lowest-power-low-jitter-retimers-for-4k-uhd-video-and-camera-interface-300287449.html
SOURCE Texas Instruments