DALLAS, Nov. 6, 2014 /PRNewswire/ -- The programmable real-time unit (PRU) on Sitara™ processors from Texas Instruments (TI) (NASDAQ: TXN) enables customers to differentiate their products by offloading real-time processing from the ARM® core. The PRU is a 200MHz low-latency multicore co-processor optimized for deterministic, real-time processing with local peripherals and memory that allows customers to save time and money by removing costly FPGAs or ASICs from system designs. The PRU offloads processing from the ARM in order to manage deterministic tasks such as time-critical I/O manipulation and is robust enough to enable complex functions like motor control in applications such as 3D printers, LED lighting control, robotics, thermal printing, and more.
The programmable nature of the PRU, along with its single-cycle direct access to I/O pins within 5ns, and SoC resources, provides flexibility in implementing fast real-time responses, specialized data handling operations, custom peripheral interfaces, and offloading tasks from the other processor cores of the system-on-chip (SoC). It also gives developers the ability to implement different interfaces including bit-banging serial interfaces like I2C and SPI, advanced PWMs, motor control, RS485, sample rate conversion and sensor monitoring for a variety of end applications.
A vast resource ecosystem
TI offers a PRU software support package that provides a framework and examples for developing software for the PRU. This package contains example PRU firmware as well as application loader code for the host OS. The examples demonstrate the PRU capabilities in order to interact with and control the system and its resources. The recently released C compiler for PRU as part of the Code Composer Studio™ integrated development environment v6 makes it easier to program the PRU and eliminates the need for assembly level programming because developers can debug over JTAG.
Introducing a new PRU cape for BeagleBone Black
The PRU cape plug-in board sold and supported by TI is an addition to capes available from the community for BeagleBone Black and gives customers an inexpensive way to evaluate the PRU capabilities on Sitara processors. The PRU cape allows easy evaluation and learning to program the dual-core PRU in AM335x processors. The code is also reusable in other Sitara processor families such as the AM437x solutions, which include a more feature rich, quad-core PRU. This cape provides access to a variety of features including basic general purpose output (GPO) via seven LEDs, general purpose input (GPI) via two push buttons, simple audio, UART, HDQ temperature sensor, GPIO header and a proto board area. Developers of the PRU will have support from TI and will be embraced by the BeagleBoard.org community. Buy the BeagleBone Black PRU cape today for $39.
For more information:
- Buy your PRU cape today
- Read this white paper on the PRU
- Download the PRU code for the Linux SDK
- Check out the PRU Cape TI Design
- Join the TI E2E™ Community
- Follow TI on Twitter
- Like TI on Facebook
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
Sitara, Code Composer Studio and TI E2E are trademarks of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.
SOURCE Texas Instruments