DALLAS, Aug. 6, 2014 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ: TXN) is advancing the infotainment and user driving experience in the automobile with seven new high-performance power management, SuperSpeed USB and logic products. TI today introduced a new power management integrated circuit (PMIC) to enhance infotainment systems. TI also introduced the industry's first USB 3.0 devices and a free-positioning Qi wireless power transmitter for automobiles that enable a more enjoyable, more convenient connected experience.
Powering next-generation infotainment systems
TI's
TPS659039-Q1
PMIC powers the DRA74x "Jacinto 6" processor and minimizes system-level power consumption in next-generation infotainment system designs. Compared to competing devices, the PMIC improves thermal management through adaptive voltage scaling, reduces electromagnetic interference (EMI) through internal and external synchronization, and enables design flexibility with power sequencing – saving board space, reducing development time and the need for an additional microcontroller.
The TPS659039-Q1 powers on in only 15 milliseconds, which gives users lightning-fast access to driver information, camera views, the navigation system and head-up display. Designers can also choose this PMIC to power dual- and quad-core ARM® Cortex-15 processors in automotive and industrial applications.
In complex infotainment systems, the new SN74AUP1T34-Q1 and TXS0102-Q1 voltage level translators solve voltage mismatch issues by simply connecting incompatible CMOS logic communication between the processor and legacy peripheral devices operating at a different voltage.
Convenient USB connectivity and wireless charging
TI's new
TUSB8041-Q1
and
TUSB8020B-Q1
USB Hub controllers and
TUS9261-Q1
USB-to-SATA bridge allow USB 3.0 connectivity for the first time in the automobile for up to four USB ports. The TUSB devices enable USB 3.0 communications capability with the 5-Gbps data flow required for multimedia applications, including mobile phones, or external hard disk drives (HDD) and solid disk drives (SDD) for applications such as portable gaming or navigation systems. The two Hub controllers' downstream ports support USB battery charging 1.2, charging downstream port (CDP), handshaking and a dedicated charging port (DCP) mode when the upstream port is not connected. The USB 3.0 Hub controllers enable USB charging and higher receive sensitivity than competing devices, reducing board space and easing system design.
The new bq500414Q is the industry's first automotive-qualified, Qi 1.1-compliant wireless power transmitter to offer free-positioning, foreign object detection and system-level EMI enhancement. The transmitter IC, which enables wireless charging from an automotive console with an A6 coil design, provides a simpler, stress-free charging experience for the driver or passengers.
Availability, packaging and pricing
All devices are shipping in volume production. They are available in the following packages and price options in 1,000-unit quantities:
- TPS659039-Q1: 169-pin, NFBGA package; US$7.60
- SN74AUP1T34-Q1: 5-pin, SC70 (DCK) package; US$0.28
- TXS0102-Q1: 8-pin, VSSOP package; US$0.38
- TUSB8020-Q1: 48-pin, QFP package; US$3.75
- TUSB8041-Q1: 64-pin, QFP package; US$5.56
- TUSB9261-Q1: 64-pin QFP package; US$5.56
- bq500414Q: 48-pin, 7-mm by 7-mm VQFN; US$3.92
Learn more about TI's automotive portfolio:
- Follow what TI automotive experts have to say on our blog: Behind the Wheel
- Download the Automotive Infotainment Guide to learn more about TI's broad analog and digital embedded and applications processing portfolio for applications such as car audio, navigation systems, power supply, as well as in-car and personal entertainment.
- Support is available on the forums in the TI E2E™ Community, where engineers can search for solutions, get help, share knowledge and solve problems with fellow engineers and TI experts.
- Analog innovation is driving the future of automotive: Check out our infographic
Texas Instruments drives automotive innovation
TI's state-of-the-art semiconductor products allow manufacturers and system suppliers to deliver world-class features to the automotive market. Our extensive automotive portfolio includes analog power management, interface and signal chain solutions, along with DLP® displays, ADAS and infotainment processors, Hercules™ TMS570 safety microcontrollers and wireless connectivity solutions. TI offers SafeTI™ parts designed to facilitate OEMs' compliance with the requirements of ISO 26262, as well as parts specifically designated as compliant with the AEC-Q100 and TS16949 standards, all with excellent product documentation. Visit TI's automotive page or TI's E2E™ Behind the Wheel Blog to learn more about our commitment to automotive innovation.
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world's brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
TI E2E is a trademark of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.
Photo - http://photos.prnewswire.com/prnh/20140806/134048
SOURCE Texas Instruments