DALLAS, June 11, 2013 /PRNewswire/ -- Texas Instruments Incorporated (TI) (NASDAQ: TXN) today introduced two tiny push-button reset controllers for space-constrained, power-sensitive applications such as pedometers, fitness bands, cell phones and tablets. The dual-channel TPS3420 and TPS3421 feature low power consumption and a selectable reset time delay to improve system stability. For more information, samples and evaluation modules, visit www.ti.com/tps3420-pr.
Push-button reset controllers are required for portable electronics with an embedded battery. In practice, the user presses and holds one or two external keys for a specific period of time, which turns the portable device off or generates a reset. The TPS3420 and TPS3421 use a long input delay to provide the intended system reset and avoid reset from short push-button or key presses. This reset configuration enables differentiation between software interrupts and hard system resets. The timers are the first in a family of new push-button controllers from TI to ensure a hard and full system reset when needed to increase efficiency.
TPS3420/1 key features and benefits
- Selectable input delay of 7.5 or 12.5 seconds eliminates unintended resets.
- Low 250-nA quiescent current conserves power for portable electronics.
- Selectable reset pulse of 400 or 800 milliseconds allows for flexible initializing.
- Small 1.45-mm by 1.0-mm by 0.55-mm SON package consumes 70 percent less board space than competitive devices.
Although TI's MSP430 microcontrollers (MCUs) are already equipped with a push-button interrupt, an external push-button reset controller, such as the TPS3420 or TPS3421, along with a voltage supervisor like the TPS3839, can serve as an extra line of security. The controller and supervisor remain isolated from the MSP430 MCU, ensuring reset as long as they are connected to a power supply. The TPS3420 and TPS3421 also relieve the MSP430 MCU of the processing power required to monitor a push-button interrupt.
TI analog for consumer electronics
TI's broad range of power management and analog signal chain products offers design engineers the high performance, low power and integration they need to create innovative and differentiated consumer electronics. TI is engineering the future with gesture recognition, touch feedback, advanced battery charging, audio, health technology and more. Learn how TI analog products improve how we live, work and play at www.ti.com/analogconsumer-pr.
Availability, packaging and pricing
The TPS3420 and TPS3421 push-button reset controllers are available in volume now from TI and its authorized distributors. Offered in a 6-pin SON package, the controllers are priced at US$0.40 in 1,000-unit quantities. For those applications requiring a single push-button input, TI offers the TPS3422 priced at US$0.34.
Find out more about TI's power portfolio:
- Ask questions and share knowledge in the Power Management forum in the TI E2E™ Community: www.ti.com/powerforum-pr.
- Download power reference designs from TI's PowerLab™ Reference Design Library: www.ti.com/powerlab-pr.
About Texas Instruments
Texas Instruments semiconductor innovations help 90,000 customers unlock the possibilities of the world as it could be – smarter, safer, greener, healthier and more fun. Our commitment to building a better future is ingrained in everything we do – from the responsible manufacturing of our semiconductors, to caring for our employees, to giving back inside our communities. This is just the beginning of our story. Learn more at www.ti.com.
Trademarks
TI E2E and PowerLab are trademarks of Texas Instruments. All other trademarks belong to their respective owners.
SOURCE Texas Instruments Incorporated