DALLAS, March 22, 2016 – Texas Instruments (TI) (NASDAQ: TXN) customers can now extend battery life in sensing and measurement applications with the new MSP430FR2311 microcontroller (MCU), the industry’s only MCU with an integrated low-leakage transimpedance amplifier (TIA) consuming just 50pA of current. The new microcontroller – an expansion of the ultra-low-power MSP430™ MCU family – offers 20 times lower leakage than alternative voltage and current sensing solutions and provides the configurability of analog and memory technology without sacrificing battery life or board space.
Highly integrated MCU solution with configurable analog helps developers simplify their schematics and save PCB space by up to 75 percent. The MSP430FR2311 MCU allows developers to connect to a wide range of sensors with its analog integration including ADC, op amp, comparators and TIA. This solution also integrates Ferroelectric Random Access Memory (FRAM) technology and eliminates the need for an onboard crystal in a single 3.5 mm x 4 mm package. This single chip solution will reduce design complexity and overall project development time.
The MSP430FR2311 MCU allows developers to choose the amplifier configuration (non-inverting, inverting or transimpedance) they need and scale their application by selecting the amount of memory to be allocated for application code or data, eliminating the boundaries of Flash to RAM ratios. Customers can get started in minutes using the MSP430FR2311 MCU LaunchPad™ development kit supported by Code Composer Studio™ integrated development environment (IDE) and IAR Embedded WorkBench®. Customers can then explore an application implementation with the MSP430FR2311 smoke sensing sub-system reference design (coming in 2Q16) using a photodiode and TIA configuration for current sensing. Additionally, customers developing for medical health and fitness, building automation and personal electronics can further extend battery life by utilizing this TI Design reference design (TIDA-00242) which uses a TI energy harvesting IC (bq25570) in an MSP430FR2311 MCU-based system.
Current MSP430G2x MCU customers using 2KB and 4KB devices can easily migrate their designs to the MSP430FR2311 MCU and take advantage of higher performance with non-volatile FRAM and higher analog integration, including operational amplifiers, ADCs and comparators. Review the MSP430F2xx and MSP430G2xx series migration guide to learn how to easily move between families when needing more analog capability.
Pricing and Availability
The MSP430FR2311 MCU is the first in a family of devices available on the TI Store for immediate sampling. These MCUs will start at USD $0.65 in 1 K unit quantities. The MSP430FR2311 MCU LaunchPad development kit is also available on the TI Store for $15.99.
Learn more about the industry’s first MCU with a configurable low-leakage TIA amplifier:
- MSP430FR2311 MCU Datasheet
- MSP-EXP430FR2311 MCU LaunchPad development kit
- MSP430FR4xx/2xx family user guide
- MSP430F2xx/G2xx to MSP430FR4xx/2xx migration guide
Inovation is at the core of TI MCUs
Beginning with the foundation of leading process technology and adding unique system architecture, intellectual property and real-world system expertise, TI continues its 20+ years of MCU innovation with low-power and performance MCUs. With unique products for ultra-low power, low-power performance and security communications, to real-time control, control and automation, and safety, designers can accelerate time to market with TI’s ecosystem of tools, software, wireless connectivity solutions, extensive Design Network offerings and technical support.
About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world’s brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.
Trademarks
MSP430 and Code Composer Studio is a trademark of Texas Instruments Incorporated. All registered trademarks and other trademarks belong to their respective owners.