DALLAS, July 7, 2020 /PRNewswire/ -- Texas Instruments (TI) (Nasdaq: TXN) today introduced the industry’s first zero-drift Hall-effect current sensors. The TMCS1100 and TMCS1101 enable the lowest drift and highest accuracy over time and temperature while providing reliable 3-kVrms isolation, which is especially important for AC or DC high-voltage systems such as industrial motor drives, solar inverters, energy-storage equipment and power supplies. For more information, see www.ti.com/TMCS1100-pr and www.ti.com/TMCS1101-pr.
Ongoing demand for higher performance in industrial systems is driving the need for more precise current measurement, in addition to reliable operation, which often comes with the cost of increased board space or design complexity. TI has applied its expertise in both isolation and high-precision analog to the TMCS1100 and TMCS1101, enabling engineers to design systems that will provide consistent performance and diagnostics over a longer device lifetime, keeping its solution size compact without increasing design time.
For more information on the TMCS1100 and TMCS1101, download the white paper, "Improving Performance in High-Voltage Systems with Zero-Drift Hall-Effect Current Sensing."
Improve system performance with the lowest drift over time and temperature
The zero-drift architecture and real-time sensitivity compensation of the TMCS1100 and TMCS1101 enable extremely high performance, even under operational conditions such as temperature changes and equipment aging. With an industry-leading total sensitivity drift over temperature of 0.45%, maximum, which is at least 200% lower than other magnetic current sensors, and a maximum full-scale offset drift of <0.1%, the devices provide the highest measurement accuracy and reliability across a wide range of current. Further, a 0.5% lifetime sensitivity drift, which is at least 100% lower than other magnetic current sensors, significantly reduces the performance degradation associated with system aging over time.
Reduce maintenance with ultra-high accuracy
Additionally, the ultra-high accuracy of the TMCS1100 (1%, maximum) and TMCS1101 (1.5%, maximum) eliminates the need for device calibration, which reduces equipment maintenance over time. The devices also provide typical linearity of 0.05%, which minimizes signal distortion and helps maintain accuracy across the extended industrial temperature range (-40°C to 125°C).
Extend system lifetime with 3-kVrms isolation in an 8-pin SOIC package
The high-quality construction of the TMCS1100 and TMCS1101 provides inherent galvanic isolation capable of delivering 3-kVrms of 60-second isolation per the Underwriters Laboratories (UL) 1577 standard for demanding environmental conditions in grid-connected or power systems. Both devices support a ±600-V lifetime working voltage – up to 40% higher than competitive devices in the same 8-pin SOIC package – and have been rigorously tested beyond industry-standard UL and VDE requirements for greater design margin and an extended device lifetime.
Meet various design needs and reduce system cost with added flexibility
The TMCS1100 requires an external voltage reference for differential measurement, enabling engineers to optimize their design to meet the most stringent performance goals. The TMCS1101, however, integrates the voltage reference, providing high performance in a pin-to-pin industry-standard implementation to simplify designs while reducing total cost.
Package, availability and pricing
The TMCS1100 and TMCS1101 are now available from TI and authorized distributors in an 8-pin small-outline integrated circuit (SOIC) package. Pricing for both sensors starts at US$1.50 in 1,000-unit quantities. Full and custom quantity reels are available on TI.com and through other channels. The TMCS1100EVM and TMCS1101EVM evaluation modules (EVMs) are available for purchase on TI.com for US$59.00 each. Multiple payment and shipping options are available on TI.com.
About Texas Instruments
Texas Instruments Incorporated (Nasdaq: TXN) has been making progress possible for decades. We are a global semiconductor company that designs, manufactures, tests and sells analog and embedded processing chips. Our approximately 80,000 products help our nearly 100,000 customers efficiently manage power, accurately sense and transmit data, and provide the core control or processing in their designs, going into markets such as industrial, automotive, personal electronics, communications equipment and enterprise systems. Our passion to create a better world by making electronics more affordable through semiconductors is alive today, as each generation of innovation builds upon the last to make our technology smaller, more efficient, more reliable and more affordable – opening new markets and making it possible for semiconductors to go into electronics everywhere. We think of this as engineering progress. It’s what we do and have been doing for decades. Learn more at TI.com.
Trademarks
All registered trademarks and other trademarks belong to their respective owners.
SOURCE Texas Instruments