New nanopower op amps maximize battery and sensor life
 

DALLAS, Nov. 9, 2016 /PRNewswire/ -- Texas Instruments (TI) (NASDAQ:TXN) today introduced the industry’s first precision nanopower operational amplifiers (op amps). The LPV811 and LPV812 consume quiescent current as low as 320 nA and are part of a family of four new ultra-low-power op amps. With up to 60 percent lower power consumption than competitive precision op amps and offset voltage as low as 300 µV, the new family of op amps extends battery and sensor life for applications such as building automation, wired and wireless sensor nodes, and wearables. For more information about the family or to order samples, see www.ti.com/nanopower-pr.

TI introduces the industry’s first precision nanopower operational amplifiers

Key features and benefits of the LPV811 family

  • Low power consumption: Featuring industry-leading quiescent current without the use of duty cycling, these nanopower op amps enable more energy-efficient 4- to 20-mA loop systems, extend battery life and reduce battery replacement costs.
  • High precision: With a precision offset voltage as low as 300 µV and nanopower current consumption, the LPV811 and LPV812 help detect low concentrations of environmental gases and increase two-lead electrochemical sensor life and sensitivity.
  • Low-voltage operation: Operating with a single-supply voltage as low as 1.6 V, the general-purpose LPV801 and LPV802 and precision LPV811 and LPV812 maintain continuous performance under low-voltage battery conditions.
  • High electromagnetic interference (EMI) immunity: An input rejection ratio greater than 80 dB in the 500-MHz to 1-GHz frequency range reduces the need for external filtering components, saves design time for EMI-sensitive applications and enables rapid system qualification according to international standards organizations.

In addition, the LPV811 family of amplifiers can drive the ADS7042 successive approximation register (SAR) analog-to-digital converter, helping to deliver an ultra-low-power analog front end.

To see a demonstration of the LPV811 precision nanopower op amp family and learn about other TI industrial and automotive innovations, visit Booth 219 in Hall A4 at the electronica Trade Fair in Munich, now through Nov. 11.

Tools and support to jump-start design

The Low Power Carbon Monoxide Sensor with 10+ Year Coin Cell Battery Life reference design demonstrates how the LPV811 nanopower op amp and the CC2650 SimpleLink™ multi-standard wireless microcontroller (MCU) reduce power consumption and extend the battery life of carbon monoxide gas detectors to as long as 10 years and extend their sensing range up to 1,000 parts per million. Designers also have access to a full suite of online support resources, including a complete library of TI Designs and SPICE models.

Package, availability and pricing

These new devices in TI’s ultra-low-power op amp portfolio are available with package types and pricing listed in the table below.

Product

Packaging

Pricing in 1,000-unit quantities

Op amp type

LPV801

5SOT-23

US$0.44

Single channel, general-purpose

LPV802

8VSSOP

US$0.70

Dual channel, general-purpose

LPV811

5SOT-23

US$0.68

Single channel, precision

LPV812

8VSSOP

US$0.95

Dual channel, precision

The LPV811 family is the latest addition to TI’s growing portfolio of innovative ultra-low-power op amps that offers a leading combination of power, efficiency and accuracy. Explore TI’s entire ultra-low-power op amp portfolio.

Learn more about TI’s op amp portfolio

About Texas Instruments

Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world’s brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks

SimpleLink is a trademark of Texas Instruments. All other trademarks and registered trademarks are the property of their respective owners.

Photo - http://photos.prnewswire.com/prnh/20161108/437138-INFO

 

SOURCE Texas Instruments

You must be logged in to view this item.

This area is reserved for members of the news media. If you qualify, please update your user profile and check the box marked "Check here to register as an accredited member of the news media". Please include any notes in the "Supporting information for media credentials" box. We will notify you of your status via e-mail in one business day.