"Jacinto 6 Entry" DRA71x processor enables high-quality display audio solutions for entry-level infotainment systems
 

DALLAS, Feb. 23, 2016 /PRNewswire/ -- Today, Texas Instruments (TI) (NASDAQ: TXN) announced the addition of an entry infotainment processor for display audio, radio/audio and other cost-sensitive in-vehicle segments to the "Jacinto 6" family of System-on-Chips (SoCs). The new DRA71x processor, "Jacinto 6 Entry," is developed on the same architecture as other "Jacinto 6" devices, enabling automotive manufacturers to scale their investment without additional R&D or significant bill of material (BOM) increases to deliver a diverse portfolio of products with hardware and software compatibility. The scalable performance within DRA71x allows developers to target specific performance for their applications and leverage headroom using higher performance variants, if required, without software modifications or hardware changes.

"Jacinto 6 Entry":  Differentiation and cost-optimization 
The DRA71x "Jacinto 6 Entry" processor is the lowest cost, feature-optimized member of the "Jacinto 6" family, extending the DRA72x "Jacinto 6 Eco" processor into more cost-sensitive applications and systems. TI’s DRA71x delivers car manufacturers with unprecedented integration of automotive features and interfaces for a processor at the entry-level of infotainment systems. As a result, the BOM is reduced and software investments leveraging the "Jacinto 6" family are protected, including high-level operating systems such as Linux, QNX and Android on ARM® Cortex®-A15 cores, as well as DSP and other cores.

TI’s DRA71x delivers an optimized set of performance and features to address the display audio and entry infotainment segments including:

  • An integrated TMS320C66x DSP for software-defined radio (SDR) integration, audio/speech processing, noise suppression and camera/imaging processing
  • Video decode/processing capability with 1080p60 decoding at greater than 30Mbps to support concurrent high-quality smartphone screen replication (including 3-D maps) and on-board video acceleration for multimedia playback
  • Highest memory bandwidth at 32-bit DDR3 EMIF at 667 MHz for a best-in-class HMI, HD display support and improved auto concurrencies
  • Integrated video ports for integrating support for NHTSA-required rear-visibility technology or other camera applications
  • ARM Cortex-M4 cores as auxiliary processors to offload high-interrupt load tasks from the main ARM core and provide physical separation between High Level Operating System (HLOS)  and real-time operating system (RTOS)

Highly scalable family of automotive processors
The "Jacinto 6" family of processors is built on the same architecture, offering software and hardware compatibility with the broadest array of highly scalable ARM® Cortex®-A15 cores for automotive applications. Other members of the "Jacinto 6" family of infotainment processors include:

  • The DRA72x, "Jacinto 6 Eco" delivering feature-rich, in-vehicle infotainment and telematics features for entry- to mid-level vehicles.
  • The DRA74x "Jacinto 6" is intended for mainstream in-vehicle infotainment applications and head-units.
  • Both DRA75x processors, "Jacinto 6 EP" and "Jacinto 6 Ex", have extended DSP and vision processing performance to enhance digital cockpit integration.

Availability
The DRA71x "Jacinto 6 Entry" processor is intended for high-volume automotive manufacturers and is not available through distributors.

For more information:

  • Learn about TI’s "Jacinto 6" family of processors.
  • Watch the video on "Jacinto 6 Entry."
  • Video the latest Behind the Wheel blog post on "Jacinto 6 Entry".
  • Read the latest Infotainment whitepaper.
  • Engage with engineers and TI experts on TI E2E Community.

Texas Instruments drives automotive innovation
TI’s state-of-the-art semiconductor products allow manufacturers and system suppliers to deliver world-class features to the automotive market. Our extensive automotive portfolio includes analog power management, interface and signal chain solutions, along with DLP® displays, ADAS and infotainment processors, Hercules™ TMS570 microcontrollers and wireless connectivity solutions. TI offers SafeTI™ parts designed to facilitate OEMs’ compliance with the requirements of ISO 26262, as well as parts specifically designated as compliant with the AEC-Q100 and TS16949 standards, all with excellent product documentation. Visit TI’s Automotive page or TI’s E2E™ Behind the Wheel Blog to learn more about our commitment to automotive innovation. 

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog ICs and embedded processors. By employing the world’s brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
All trademarks are the property of their respective owners.

 

SOURCE Texas Instruments Incorporated (TI)

You must be logged in to view this item.

This area is reserved for members of the news media. If you qualify, please update your user profile and check the box marked "Check here to register as an accredited member of the news media". Please include any notes in the "Supporting information for media credentials" box. We will notify you of your status via e-mail in one business day.