Oct 06, 2020

Journey of innovation

A “Just do It” attitude is exactly what was required of the TI mmWave R&D team during their nine-year innovation journey to create a technology that made it possible to integrate affordable mmWave radar systems into mid-to-low-end vehicles to improve safety. This is the inside story.

Sep 29, 2020

Vision: Possible

Imagine a low-cost radar sensor that could be affixed to a firefighter's helmet to detect an unconscious or incapacitated person through walls and smoke. Thanks to our company's engineers who created the world's first millimeter-wave radar system on chip, our customers can integrate radar sensing technology into an array of applications that improve safety on the road and in factories, and could even help firefighters save lives.

Jan 08, 2019

5 ways your drive is changing faster than the autobahn

From enhanced connectivity, adaptive features and new levels of personalization, innovations and advancements in sensors, processors, microcontrollers, DLP® technology are changing your driving experience today and in the near future. 

Sep 18, 2018

Intelligent autonomy at the edge: Sensors making decisions on their own can make life smarter

With a microcontroller, a radio-frequency front end, a hardware accelerator and a programmable DSP, TI mmWave sensors calculate an object's range, velocity and angle at up to three times higher resolution than any other radar sensor on the market.

Jun 12, 2018

Chief Technology Officer Ahmad Bahai discusses how TI mmWave technology helps us see clearly

Many technology leaders have long dreamed of a highly integrated radar vision that is accurate and uncluttered by ambient noise. TI mmWave sensors can see objects with detailed outlines and classify them.