DLP3310 DMD and DLPC3437 controller combine size, efficiency and performance to deliver an industry-leading display solution for mobile smart TVs, pico projectors, smart home displays and more
 

DALLAS, Jan. 25, 2017 /PRNewswire/ -- As brands and developers have been eagerly awaiting a solution that will allow them to create smaller form factor products integrating 1080p projection displays, Texas Instruments (TI) (NASDAQ: TXN) today announced its DLP Pico 0.33-inch full-HD chipset. Consisting of the DLP3310 digital micromirror device (DMD) and DLPC3437 controller, this is the industry’s smallest 1080p display chip solution with the highest brightness capabilities in the 0.3-inch imager class. This latest DLP offering continues TI’s commitment to enabling smaller form factors, superior image quality and high system efficiency for customers designing and integrating pico displays. For more information, visit www.ti.com/dlp3310.

With the 0.33-inch chipset, developers can create a myriad of compact, portable display applications, such as mobile smart TVs, battery-operated pico projectors, smart home projection displays, signage and industrial solutions.

Key features and benefits of the 0.33-inch full-HD chipset:

  • Small form factor 1080p: The fast switching speed of the DMD enables each mirror to display two distinct and unique pixels on screen during every frame. This DLP solution delivers 1080p resolution to the screen along with the industry’s highest brightness capability for its size class, enabling a powerful new combination for developers of compact display products.
  • Crisp images and video: Proven DLP technology delivers high color fidelity (up to 16M colors) for vibrant, beautiful images.
  • Power efficiency: This latest DLP chipset offers efficiency to meet the growing demand of battery powered devices adding display capability 

TI collaborates with the most extensive ecosystem of pico optical engine manufacturers in the industry. This offers developers a path to production-ready optical engines, which helps reduce design time and gets customers’ innovative products to market faster. Manufacturers planning to offer an optical module utilizing DLP3310 include Shenzhen Anhua Optoelectronics Technology Co. Ltd, Coretronic Corporation, DigitalOptics Co. Ltd, Ongine Technology, Young Optics, Inc. and others.

Availability

The 0.33-inch full-HD chipset and the associated components1 will be available in 2H17. For more information, or to sign up for DLP3310 notifications visit www.ti.com/dlp3310

Find out more

About Texas Instruments DLP Products
Since 1996, award-winning TI DLP technology has powered the world’s top display devices to deliver high-resolution images rich with color, contrast, clarity and brightness for a wide range of applications, including industrial, automotive, medical and consumer market segments. DLP technology is being used in movie theatres (DLP Cinema® products) and large-scale, professional venues and conference rooms, classrooms and home theaters. With mobile devices enabled by DLP® Pico technology, users have the ability to display images from the palm of their hand. Every DLP chipset features an array of microscopic mirrors that switch on and off up to 10,000 times per second. To learn more, please visit www.ti.com/dlp or follow TI DLP technology on Twitter at @TI_DLP.

About Texas Instruments
Texas Instruments Incorporated (TI) is a global semiconductor design and manufacturing company that develops analog integrated circuits (ICs) and embedded processors. By employing the world’s brightest minds, TI creates innovations that shape the future of technology. TI is helping more than 100,000 customers transform the future, today. Learn more at www.ti.com.

Trademarks
DLP and DLP Cinema are registered trademarks and DLP Pico and IntelliBright are trademarks of Texas Instruments. All registered trademarks and other trademarks belong to their respective owners.

1 *FPGA- Xilinx XC7Z020-1CLG484I4493, PMIC- TI DLPA3000

 

 

SOURCE Texas Instruments (TI)